the downloaded MDB file for S32K1xx is broken

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

the downloaded MDB file for S32K1xx is broken

1,094 Views
jackjack
Contributor III

2.png2019-01-26_185829.png

the downloaded MDB for S32K1xx is not an exe file after i decompressed the file, shouldn't that be an exe file?

as far as i know, MBD for MPC574x is an exe file.

Labels (3)
Tags (2)
0 Kudos
1 Reply

916 Views
constantinrazva
NXP Employee
NXP Employee

Hello jackjack‌,

Our older versions of the toolbox have installers (.exe format), but our newer versions use MATLAB mltbx format. This format has been introduced to make distribution of toolboxes easy. All you have to do is open the .mltbx file with MATLAB and follow the instructions that pop-up.

The file itself is a zip-file, but has a preset configuration so that MATLAB add-on manager knows how to install it. It has a folder fsroot that holds all the files within the toolbox.

You can use this video as a walk-through for the installation - it is for a previous version, but it uses the new format 'installer' - the .mltbx file.

Hope this helps,

Razvan.

0 Kudos