gpio_s32k14_output block (mask) does not have a parameter named 'port'

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

gpio_s32k14_output block (mask) does not have a parameter named 'port'

658 次查看
1586526941
Contributor I

gpio_s32k14_output block (mask) does not have a parameter named 'port',How to solve this problem?

0 项奖励
2 回复数

583 次查看
constantinrazva
NXP Employee
NXP Employee

Hello 1586526941@qq.com‌,

Can you provide the example you are trying to build?

A few more questions to get a better understanding of the context - do you have the correct path set ? Do you have multiple toolboxes installed ? Maybe more versions of the S32K toolbox?

Can you send me the output of the following MATLAB command:

ver

Kind regards,

Razvan.

0 项奖励

583 次查看
1586526941
Contributor I

hi

    the toolbox version is MBDToolbox S32K1xx_2018.R1_20180723.mltbx,when the Dightal_Output is existing,to load the Write_Register, this problem will arise.

0 项奖励