MBDT installer for S32S HCP

Hi, I'm trying to install the HCP 1.0.0 EAR, and when downloading the *.mltbx, I get a zip file containing a directory structure with various files, but no *.mltbx.
Flexera link: Design : Product Download : Files (flexnetoperations.com)
File I'm trying to download: SW32_MBDT_HCP_1.0.0.EAR_D2111.mltbx
File I actually download: SW32_MBDT_HCP_1.0.0.EAR_D2111.zip
Contents of the file I downloaded:
C:\mw_hcp_1_0_0\SW32_MBDT_HCP_1.0.0.EAR_D2111>dir
Volume in drive C has no label.
Volume Serial Number is 48D5-EB3A
Directory of C:\mw_hcp_1_0_0\SW32_MBDT_HCP_1.0.0.EAR_D2111
11/06/2021 08:24 AM <DIR> .
11/06/2021 08:24 AM <DIR> ..
11/06/2021 08:24 AM <DIR> fsroot
11/06/2021 08:24 AM <DIR> metadata
11/06/2021 08:24 AM 159,068 [Content_Types].xml
11/06/2021 08:24 AM <DIR> _rels
11/06/2021 08:24 AM <DIR> _xmlsignatures
1 File(s) 159,068 bytes
6 Dir(s) 49,176,612,864 bytes free
There is no SW32_MBDT_HCP_1.0.0.EAR_D2111.mltbx in the zip file.

I found the answer on the download page:
"The NXP Model-Based Design Toolbox is delivered as a MATLAB MLTBX file. If your browser download the file as a zip, simply change the file extension back to *.mltbx to be recognized by MATLAB Installer"
This issue can be closed.


Hi @curt_hillier,
Indeed, there is a limitation with the hosting platform I guess, for the mltbx file it downloads the installer as zip. But, by just changing the extension back to mltbx, MATLAB can recognize the file and install the toolbox as you may have already proceeded.
Regards,
Marius