Executing PIL with the S32K114 evaluation board on an integrated model level

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Executing PIL with the S32K114 evaluation board on an integrated model level

347 Views
oashraf96
Contributor II

I have been successful in using the profiler function and executing PIL using S32K114 on a component level and getting back tick measurements.

The main issue I am facing right now is using PIL on an integrated level with different components (Using Model Reference Block) and operating with different periodicities.

How can I correctly set up the integrated model in order to be capable of getting profiler results back?

What are the correct steps the fully operate PIL on the integrated level and what are the constraints I should take care of and overall best practices that should be considered.

 

 

Note that I am using a specific architecture in which I run MIL/SIL in:

1 - The top level is a model reference of a subsystem accompanied by a state-chart that triggers events that acts as an executor of the components.

2 - The subsystem model above contains model references of all other components and not mere subsystems.

 

Works for MIL/SIL but not PIL

I fully intend to understand the variables in order to automate PIL on other Simulink projects.

 

Thank You

 

Labels (1)
0 Kudos
0 Replies