I found LF_v5.10.72-2.2.0_images_IMX6QPDLSOLOX.zip, but there is no sdcard image, so where and how do I find a up to date sdcard image for a "15a2:0054 Freescale Semiconductor, Inc. i.MX 6Dual/6Quad SystemOnChip in RecoveryMode"
On board I find MCIMX6q-sdb, SCH-27516 Rev C4, 700-27516 Rev B
I tried using uuu to install LF_v5.10.72-2.2.0_images_IMX6QPDLSOLOX.zip and it failed. So I figure that the board is too old to use uuu, so I am trying to build a new sdcard to put the latest and greatest code, and then try to use uuu to install LF_v5.10.72-2.2.0_images_IMX6QPDLSOLOX.zip into emmc and continue from there.
Also can you give a pointer to the right sdk/git tag for doing yacto builds. Have not found that either,
Maybe the board is too old to use, I assume you will tell me.
Terry
Hello,
Yes, this board it is still supported, but note that .sdcard format it Is not used anymore in our releases we use the .wic format but the usage is the same so no issue there.
Regarding on using UUU you may try with the following command:
uuu -V .\LF_v5.10.72-2.2.0_images_IMX6QPDLSOLOX.zip\uuu.auto-imx6qsabresd
Best regards,
Aldo,