Hi,
I am building a project that is based on platform KDS3.0 +KSDK1.2+PEx.
I am using MQXLite OS. It is not allow me to enable mutex. It said it doesnt
support. I have to run multi threads with some shared variables. Is there
any way that I can get around this issue?
Thanks,
Yaran
已解决! 转到解答。
Hi Yaran:
Here is a document to enable MQX Lite in KSDK1.1 , you can choose "mutexes" component to enable mutex, and rebuild all.
How To: Create an MQX RTOS for KSDK project with Processor Expert in Kinetis Design Studio IDE
I tried it with KSDK1.3 , it seems mutex is hidden in this version, it only suuport lightweight events and lightweight message queues in this version
Regards
Daniel
Hi Yaran:
MQX Lite supports lightweight subset of the MQX componets: LW semaphore, LW evet, Mutex, LW message.
There is an example using mutex
C:\Freescale\CW MCU v10.6\MCU\CodeWarrior_Examples\Processor_Expert\MQXLite\Kinetis\FRDM_KL25Z\MUTEX_KL25Z
Mutex is an optional component, the default state is disable.
I think if you add the below line into user_config.h, and recompile all. it should able to support mutex.
#define MQX_USE_MUTEXES | 1 |
I am attaching the mqxlite user manual here.
Regards
I did that and it threw me error when I run the program. It said
Description | Resource | Path | Location | Type |
#error MUTEX component is currently disabled in MQX kernel. Please set MQX_USE_MUTEXES to 1 in mqx_sdk_config.h and recompile kernel. | mutex.h | /shiny_v3/SDK/rtos/mqx/mqx/source/include | line 36 | C/C++ Problem |
So how would i be able to recompile the kernel from KDS?
Thanks,
Hi Yaran:
Here is a document to enable MQX Lite in KSDK1.1 , you can choose "mutexes" component to enable mutex, and rebuild all.
How To: Create an MQX RTOS for KSDK project with Processor Expert in Kinetis Design Studio IDE
I tried it with KSDK1.3 , it seems mutex is hidden in this version, it only suuport lightweight events and lightweight message queues in this version
Regards
Daniel