RS485 on MQX 4.0 Port change

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

RS485 on MQX 4.0 Port change

1,098 次查看
yogesh8418
Contributor III

I am a new to Tower system with codewarrior  and MQX. I have TWR-K20D72M and TWR-IND-IO. I am trying to use RS-485 port  From MQX example.

I want Know That If I want to change the UART Port in the example For example UART1 to UART2.

HOw can I do It . I dont understand On which port RS-485 is working .I am using the code below.

/**HEADER********************************************************************

*

* Copyright (c) 2008 Freescale Semiconductor;

* All Rights Reserved                      

*

* Copyright (c) 1989-2008 ARC International;

* All Rights Reserved

*

***************************************************************************

*

* THIS SOFTWARE IS PROVIDED BY FREESCALE "AS IS" AND ANY EXPRESSED OR

* IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES

* OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. 

* IN NO EVENT SHALL FREESCALE OR ITS CONTRIBUTORS BE LIABLE FOR ANY DIRECT,

* INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES

* (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR

* SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION)

* HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT,

* STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING

* IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF

* THE POSSIBILITY OF SUCH DAMAGE.

*

**************************************************************************

*

* $FileName: rs485.c$

* $Version : 3.8.4.0$

* $Date    : Oct-4-2011$

*

* Comments:

*

*   This file contains the source for the rs485 example program.

*

*END************************************************************************/

#include <mqx.h>

#include <bsp.h>

#include <fio.h>

#include <string.h>

#if ! BSPCFG_ENABLE_IO_SUBSYSTEM

#error This application requires BSPCFG_ENABLE_IO_SUBSYSTEM defined non-zero in user_config.h. Please recompile BSP with this option.

#endif

/* select if example transmit, or receive

** 1 transmit

** 0 receive

*/

#define RS485_TRANSMIT  1

/* enable if device has RTS pin hw support */

#define HAS_485_HW_FLOW_CONTROL 1

/* set RS485 output device */

#define RS485_CHANNEL "ittyd:"

/* Task IDs */

#define RS485_TASK 5

extern void rs485_write_task(uint_32);

extern void rs485_read_task(uint_32);

const TASK_TEMPLATE_STRUCT  MQX_template_list[] =

{

   /* Task Index,   Function,         Stack,  Priority, Name,     Attributes,          Param, Time Slice */

#if (RS485_TRANSMIT == 1 )

   { RS485_TASK,   rs485_write_task,  1500,   8,        "rs_485", MQX_AUTO_START_TASK, 0,     0 },

#else

   { RS485_TASK,   rs485_read_task,   1500,   8,        "rs_485", MQX_AUTO_START_TASK, 0,     0 },

#endif

    { 0 }

};

/*TASK*-----------------------------------------------------

*

* Task Name    : rs485_write_task

* Comments     :

*    This task send data_buffer to rs485

*

*END*-----------------------------------------------------*/

void rs485_write_task

   (

      uint_32 initial_data

   )

{

   MQX_FILE_PTR rs485_dev = NULL;

   char  data_buffer[] = "RS485 send example";

   boolean disable_rx = TRUE;

   uint_32 result;

   /* If mcu has hardware support for RTS pin drive (e.g. k60n512), open line with IO_SERIAL_HW_485_FLOW_CONTROL flag */

   #if (HAS_485_HW_FLOW_CONTROL) 

   /* HW 485 flow control on chip*/

   rs485_dev = fopen( RS485_CHANNEL, (char const *)IO_SERIAL_HW_485_FLOW_CONTROL );

   #else

   /* HW 485 flow not available on chip */

   rs485_dev  = fopen( RS485_CHANNEL, NULL );                     

   #endif

  

   if( rs485_dev == NULL )

   {

      /* device could not be opened */

      _task_block();

   }

  

   /* half duplex, two wire. use only if disable receiver in transmit is desired */

   result = ioctl( rs485_dev, IO_IOCTL_SERIAL_DISABLE_RX, &disable_rx );

   if( result == IO_ERROR_INVALID_IOCTL_CMD )

   {

      /* ioctl not supported, use newer MQX version */

      _task_block();

   }

  

   #if !(HAS_485_HW_FLOW_CONTROL)

   /* User written function for flow control by GPIO pin - handle RTS other signal to drive RS485 HW driver */

   #endif

  

   /* write data */

   write( rs485_dev, data_buffer, strlen(data_buffer) );

  

   /* empty queue - not needed for polled mode */

   fflush( rs485_dev );

  

   /* wait for transfer complete flag */

   result = ioctl( rs485_dev, IO_IOCTL_SERIAL_WAIT_FOR_TC, NULL );

   if( result == IO_ERROR_INVALID_IOCTL_CMD )

   {

      /* ioctl not supported, use newer MQX version */

      _task_block();

   }

  

   /* half duplex, two wire */

   /* if receiver was disabled before, enable receiver again */ 

   disable_rx = FALSE;

   ioctl( rs485_dev, IO_IOCTL_SERIAL_DISABLE_RX, &disable_rx ) ;

  

   #if !( HAS_485_HW_FLOW_CONTROL )

   /* User written function for flow control by GPIO pin - handle RTS */

   #endif

   _task_block();

}

/*TASK*-----------------------------------------------------

*

* Task Name    : rs485_read_task

* Comments     :

*    This task send data_buffer to rs485

*

*END*-----------------------------------------------------*/

void rs485_read_task

   (

      uint_32 initial_data

   )

{

   MQX_FILE_PTR rs485_dev = NULL;

   char  data_buffer[256];

   rs485_dev  = fopen( RS485_CHANNEL, NULL );                     

   if( rs485_dev == NULL )

   {

      /* device could not be opened */

      _task_block();

   }  

  

   /* wait for data */

   fread(data_buffer, 1, 18, rs485_dev);

  

   while(1)

   {    

    printf("\n - Buffer_DAta              = %s Hz", &data_buffer);

   };

}

/* EOF */

Please Help

0 项奖励
1 回复

341 次查看
danielchai
Senior Contributor I

Hi,

I think "#define RS485_CHANNEL "ittyd:" defined which UART you want to use.

For example: "ttya:" is polled uart0 "ittya:" is interrupt driven uart0. "ttyb:" is uart1.

0 项奖励