Porting Kinetis BSP_pe from MQX 3.7 to MQX 3.8.1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Porting Kinetis BSP_pe from MQX 3.7 to MQX 3.8.1

434 Views
Vagni
Contributor IV

I developed my application with CodeWarrior 10.2 and MQX 3.7 on my K60-based custom board.

I cloned the original bsp_twrk60n512_pe BSP library, based on Processor Expert embedded components, to have my BSP_pe library for my board.

My application is working properly, but now I need to add more functionalities (i.e. USB and Ethernet) and I am thinking to port my project from MQX 3.7 to MQX 3.8.1.

 

I installed the last MQX 3.8.1 version and I see there is only one bsp_twrk60n512 BSP project. What was changed?

 

I need a step-by-step procedure to port my working BSP_pe library to be compiled with MQX 3.8.1, without having to remake again all the Processor Expert drivers my custom board needs.

I hope it is possible ...

 

I was thinking to clone bsp_twrk60n512 BSP project for my board and then add all the Processor Expert files (project, code generated files, etc.). Is it the right way?

 

 

 

 

0 Kudos
1 Reply

209 Views
ProcessorExpert
Senior Contributor III

Hi,

 

I was informed that newly in MQX 3.8.1 all BPSs are PE ready and the old BSPs with _pe are no more distributed with MQX and should not be used (you may encounter  issues with compiling). 

 

best regards
Petr Hradsky
Processor Expert Support Team

 


0 Kudos