I'm working on a custom board based on the K21F120M tower board, and I'm not seeing the expected activity on the SPI bus. I think it is related to the pin MUX selections for the SPI but I'm not sure where that's defined. I'm using SPI0 on pins 93-96 (100pin package), but I'm not sure if the MUX options are set correctly, or how you even define which pins to use.
From _bsp_dspi_io_init () in init_gpio.c, it seems that for SPI0 it is defining I/O pins D0-D3, which is the same ones used on the tower board and also the ones I'm using, but it doesn't seem to work right. Am I missing something?
I'm also not clear about whether I should have DSPI0_USE_DMA selected. Are BSPCFG_DPSI0_USE_DMA and BSPCFG_ENABLE_SPI0 mutually exclusive? When they refer to DSPI in the MCU reference manual, does this mean DMA SPI?
Thanks,
Angelo
已解决! 转到解答。
Hi Angelo,
Please check the attached document. There is a section that includes add a new pin to the BSP which is the section that I believe you will find useful.
Have a great day,
Sol
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Angelo,
Please check the attached document. There is a section that includes add a new pin to the BSP which is the section that I believe you will find useful.
Have a great day,
Sol
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------