MQX and MPU

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
576件の閲覧回数
salerio
Contributor I

Does anyone know if the current version of MQX (3.5 i think) supports the MPU in the Kinetis Cortex M4 devices. I would like if possible to segregate some tasks stacks from each other in my application.

0 件の賞賛
1 解決策
277件の閲覧回数
ColoPaul
Contributor II

Actually, the current version is 3.8.0;  I've heard rumors that a 3.8.1 beta exists.

There is no support for the MPU.   Maybe it is coming?

In the release notes for 3.8.0 there is the following text:

 

The CortexM PSP (Kinetis kernel) has been modified to be able to create tasks running in user (restricted) mode. The lightweight memory management, dynamic task creation, lightweight semaphore, event and message API functions were implemented to operate from user mode. This is an experimental prototype of the feature available for K60 and IAR build tools only in this version.

元の投稿で解決策を見る

0 件の賞賛
1 返信
278件の閲覧回数
ColoPaul
Contributor II

Actually, the current version is 3.8.0;  I've heard rumors that a 3.8.1 beta exists.

There is no support for the MPU.   Maybe it is coming?

In the release notes for 3.8.0 there is the following text:

 

The CortexM PSP (Kinetis kernel) has been modified to be able to create tasks running in user (restricted) mode. The lightweight memory management, dynamic task creation, lightweight semaphore, event and message API functions were implemented to operate from user mode. This is an experimental prototype of the feature available for K60 and IAR build tools only in this version.

0 件の賞賛