MQX/MQX Lite Context Switching Cycles

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MQX/MQX Lite Context Switching Cycles

ソリューションへジャンプ
609件の閲覧回数
MatthewScott_DE
Contributor II

Does anyone know the amount of cycles it takes to perform a context switch in MQX?  Is MQX Lite any different?

タグ(3)
0 件の賞賛
1 解決策
267件の閲覧回数
c0170
Senior Contributor III

Hello,

this thread gives you a hint which example to check and david shared also there some numbers:

Re: Minimum Interrupt Latency

Quoted from MQX Real-time Operating System

Depending on platform and options chosen, MQX RTOS can be configured to take as little as 6K bytes of ROM, including kernel, interrupts, semaphores, queues and memory manager. MQX RTOS delivers the performance that demanding customer have come to expect in leading RTOS solutions as well, on a 200 MHz PowerPC® MPC8248, interrupt latency came in at 0.331 µsec and context switch time was benchmarked at 0.558 µsec.

Regards,

c0170

元の投稿で解決策を見る

0 件の賞賛
1 返信
268件の閲覧回数
c0170
Senior Contributor III

Hello,

this thread gives you a hint which example to check and david shared also there some numbers:

Re: Minimum Interrupt Latency

Quoted from MQX Real-time Operating System

Depending on platform and options chosen, MQX RTOS can be configured to take as little as 6K bytes of ROM, including kernel, interrupts, semaphores, queues and memory manager. MQX RTOS delivers the performance that demanding customer have come to expect in leading RTOS solutions as well, on a 200 MHz PowerPC® MPC8248, interrupt latency came in at 0.331 µsec and context switch time was benchmarked at 0.558 µsec.

Regards,

c0170

0 件の賞賛