MQX 5.2 K60 fsl_flexcan

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MQX 5.2 K60 fsl_flexcan

1,350件の閲覧回数
jjt
Contributor I

I inherited a MQX 4.2 project using the fsl_flexcan driver. Our application was running fairly well but during testing we rediscovered the CAN rx fifo bug (that dates back to 2015). I figured out a fix around this bug but seeing that MQX 4 is no longer supported, I recommended we upgrade to MQX5 rather than invest time on an unsupported OS.

I'm regretting this recommendation as MQX5, at least on the K60, doesn't seem like it has much support evidenced by taking almost 3 weeks after placing the order to get a set of files that don't even include the fsl_flexcan driver. 

Q1) Is there an update to the fsl_flexcan driver that fixes the rxfifo bug? 

0 件の賞賛
2 返答(返信)

1,339件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi 

 

I remember for TWR-K60F120M, MQX 4.2 is using the old flexcan driver, hardware rxfifo is not enabled.  For TWR-K70F120M, rxfifo is enabled.

I would suggest you use Processor Expert routine that comes with Code Warrior. It should can generate CAN rx fifo code.

 

Regards

Daniel

 

0 件の賞賛

1,346件の閲覧回数
jjt
Contributor I

ok, I found the fsl_flexcan driver files in the directory. I will add these to the project and see if the bug has been fixed in this code.

0 件の賞賛