Looking for a DNS client / DHCP client example

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Looking for a DNS client / DHCP client example

跳至解决方案
5,036 次查看
vier_kuifjes
Senior Contributor I

I have a Coldfire Lite based application that I would like to try to port to MQX. This application works as a HTTP client (not a HTTP server as in most demo apps).

 

There is a lot of MQX documentation available, which I'm reading, but some practical examples are sometimes more useful. Can someone provide me with some working code examples of a DHCP client and DNS client?

 

Any help is much appreciated!

标签 (1)
标记 (1)
1 解答
1,389 次查看
EAI
Contributor IV
Many of the examples provided in the releaseare configured with DHCP and DNS clients. You can look at demo\security_email\security_network.c as one example.

在原帖中查看解决方案

5 回复数
1,390 次查看
EAI
Contributor IV
Many of the examples provided in the releaseare configured with DHCP and DNS clients. You can look at demo\security_email\security_network.c as one example.
1,389 次查看
AloysiusJegan
Contributor III

Thanks for the info. I implemented in my project and it is working fine.

 

 

Regards

Aloysius Jegan

 

http://www.aloysiusjegan.in

 

 

 

0 项奖励
回复
1,389 次查看
vier_kuifjes
Senior Contributor I

Thanks.

 

Is this file actually being used in any of the demo projects? There doesn't appear to be a .mcp file  in the security_* folders...

0 项奖励
回复
1,389 次查看
vier_kuifjes
Senior Contributor I
Anyone?
0 项奖励
回复
1,389 次查看
AloysiusJegan
Contributor III

Anyone?????????

Even I also want the same...

 

 

-AJ

 

http://www.aloysiusjegan.in

0 项奖励
回复