Has anyone had FTDI Usb Host functionality working on MQX?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Has anyone had FTDI Usb Host functionality working on MQX?

ソリューションへジャンプ
945件の閲覧回数
danielwinsor
Contributor II

I used the CDC driver, added a class definition as follows:

// USB2SERIAL (FT232R USB-Serial (UART) IC )
{{0x00,0x00}, {0x00,0x00}, USB_PROTOCOL_COM_VENDOR, 0, 0, 0, CUsbHostManager::UsbHostEvent },

// USB Data
{{0x00,0x00}, {0x00,0x00}, USB_CLASS_DATA, 0xFF, USB_PROTOCOL_DATA_CDC, 0, CUsbHostManager::UsbHostDataEvent },

I get an attach and detach calls when I plug the device in, but when I call these two functions they fail:

if (USB_OK != usb_class_cdc_get_acm_descriptors(dev_handle,
intf_handle,
&acm_desc,
&cm_desc,
&header_desc,
&union_desc))
{
break;
}

if (USB_OK != _usb_hostdev_select_interface(dev_handle, intf_handle, (pointer) & device_info[ulDeviceIndex].ccs))
{
break;
}

Is there a completed FTDI (FT232RQ device) driver code for usb host?

Thanks!

Dan.

ラベル(1)
0 件の賞賛
返信
1 解決策
650件の閲覧回数
danielwinsor
Contributor II

gave up with ftdi.  got a MCP2200 usb to serial device (supports CDC)

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
651件の閲覧回数
danielwinsor
Contributor II

gave up with ftdi.  got a MCP2200 usb to serial device (supports CDC)

0 件の賞賛
返信