Freescale MQX™ 4.1.2 GA for Vybrid release

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Freescale MQX™ 4.1.2 GA for Vybrid release

Freescale MQX™ 4.1.2 GA for Vybrid release

The new Freescale MQX™ 4.1.2 GA for Vybrid release is now available on www.freescale.com/mqxrtos

·      Files available

         

       

#

Name

Description

1

Freescale MQX RTOS 4.1.2 for Vybrid Linux Base

This   release has the same basic code as the 4.1.2 version, with just the changes   needed to build and debug on Linux systems.

2

Freescale MQX RTOS 4.1.2 for Vybrid

MQX™ Source   code. Includes an RTOS, File System, TCP/IP and USB host/device software   stacks. Does not require MQX™ 4.1.1 installation.

·         What is New?

·         New Board Support Package

·         X-SVF522R-EVB Vybrid Evaluation Board Rev. B with the SVF522R3MK4 processor.

·         TWR-VF65GS10 Development Kit Rev. H with the MVF61NS10MK50 processor.

·         New Features and Updates

·         BSP package for TWR-VF600 was replaced by new TWR-VF65GS10

·         Vybrid Auto EVB board was replaced by new X-SVF522R-EVB board

·         MFS library was updated

·         New USB stack was added

·         Exception support for cortex A kernel

·         Video ADC + VIU example application

·         RTCS package was updated

·         Known issues

·         For known issues and limitations please consult the release notes

タグ(2)
評価なし
バージョン履歴
最終更新日:
‎12-05-2014 03:41 PM
更新者: