Hello everyone,
I'm using S32DS 1.2 to develop demo which want use CANFD to transfer data.
When I run the demo , the demo was cycling in FLEXCAN_SetStuffBitCount function, I use the PE to generate code automatically.
and then i found here is a defination for E8759:
Does that mean I should comment it out to use CANFD? If not ,how to configure it?
Hi,
if the MCU has mask set N78S then you can simply comment #define ERRATA_E8759.
If you have older mask 1N81M you should not use CAN FD unless all devices on the bus comply with older CAN FD standard.
BR, Petr