could MPC5746C slave DSPI2 correct clock/bit skew error on next comming CS period

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

could MPC5746C slave DSPI2 correct clock/bit skew error on next comming CS period

765 次查看
wesleyxie
Contributor III

Hi, NXP guys

khumphriMandardhavalRHinnenjimtrudeauMartinvladcenteamarc.paquetteRChapmanAlban

on our board design, the MPC5746C play as a SPI slave (DSPI2), and the SPI master is IMX6.d.

I am wondering if a clock/bit skew error occured in one CS period on the SPI bus (which may caused by electronic jamming or Master start sending data before Slave ready ), will this error still exist in the next CS period ?

I understand the Rx / Tx datas on the MPC5746C(slave) side will goes wrong if clock/bit skew occured in current CS period,

but can the MPC5746C Rx / Tx correct datas on the next comming CS (CS deasserted and then asserted) without  Application software doing anything ?

if yes, could you please explain how it works ?

if not, could you please teach me how to fix this issue ?

thanks and best regards.

pastedImage_2.png

标签 (1)
0 项奖励
1 回复

556 次查看
wesleyxie
Contributor III

Hello, any comments ?

0 项奖励