Dear all,
Now, I want to know that which clock is used for DSPI's protocol clock in MPC5744.
Could anyone teach me it?
In the Figure 2-8 at Page 116(Page 117 in the PDF file) in MPC5744P Reference Manual(REV6.1)(https://www.nxp.com/docs/en/reference-manual/MPC5744PRM.pdf), the PBRIDGEx_CLK are supplied to DSPI(4).
And the word "Protocol Clock" is nothing in the DSPI(4) box.
The maximum frequency of PBRIDGE_0, PBRIDGE_1 is defined to 50MHz in the Table 13-2 in Page 339(Page 701 in the PDF file ).
But the fp(the protocol clock) is described with 100MHz or 20MHz as the example in the Table 49-5 at Page 1609(Page 1971 in the PDF file).
Is the other clock used for the protocol clock of DSPI?
Hi,
PBRIDGEx_CLK is used as protocol clock for DSPI modules.
The fp mentioned in Table 49-5 is just an example and a note below a table gives a notice about this.
BR, Petr
Dear Petr,
Thank you for your quick answer.
I had misunderstand that the MPC5744 might be able to use until 25Mbps such as Table 49-12 in page 1628(Page 1990 in PDF file).
And I understand that MPC5744 maximum baudrate is 12.5Mbps(=50MHz/2/2).
A little disappointing.
Br, Abe.