What is the maximum rate of MPC5748G as an SPI slave

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the maximum rate of MPC5748G as an SPI slave

Jump to solution
981 Views
jacst
Contributor II

We are using the MPC5748G chip as an SPI slave. What is the maximum speed? grateful

0 Kudos
1 Solution
940 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

please create new case here:

https://support.nxp.com/

This needs to be assigned to another team.

Thanks,

Lukas

View solution in original post

0 Kudos
4 Replies
947 Views
jacst
Contributor II
0 Kudos
972 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

let me copy here from the datasheet:

lukaszadrapa_0-1638369646641.pnglukaszadrapa_1-1638369681301.png

 

And something was already discussed here:

https://community.nxp.com/t5/MPC5xxx/In-SPI-i-am-able-to-reach-a-max-baud-rate-of-2mbps/td-p/1185345

Regards,

Lukas

 

0 Kudos
948 Views
jacst
Contributor II

Problem description: We use the 5748G chip as a slave node to interact with 3A through SPI. When the communication rate is 1M, it can run stably. When the communication rate is 2M, unexpected bytes will be inserted into the SPI data sent by the MCU. Cause data analysis to fail.

Is this due to the wrong EB configuration mode? There is still a problem with the underlying MCAL driver. Looking forward to reply.

Please refer to the attachment

0 Kudos
941 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

please create new case here:

https://support.nxp.com/

This needs to be assigned to another team.

Thanks,

Lukas

0 Kudos