Using EMIOS0 is to capture or PWM for different cycles

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using EMIOS0 is to capture or PWM for different cycles

762件の閲覧回数
thomasbao
Contributor II

hello, everyone:

    I want to use eMIOS_0[13] generate PWM(30 ms), and to use eMIOS_0[12] as input capture in interrupt mode(120 ms). How should it to be implemented?

タグ(2)
0 件の賞賛
3 返答(返信)

752件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

you can refer to emios demo example within S32DS and modify it per your need

PetrS_0-1629789237793.png

 

BR, Petr

 

0 件の賞賛

748件の閲覧回数
thomasbao
Contributor II

Hi Petr,

    Thank you for your reply. And I wonder if I can implement this feature directly using the SDK ?

0 件の賞賛

745件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

yes, the SDK driver can be used as well and "ic", "pwm" examples are available too

PetrS_0-1629800521359.png

 

BR, Petr

0 件の賞賛