Dear everyone,
I am using S32DS working on MPC5748G.
I am using the LWIP project in the example, and debugged it in Flash but every time I reboot it doesn't run .
I would like to ask what is the cause of this problem?
Thanks and best regards,
Li Xu
Hello,
What do you mean by reboot? Reset the device?
What does it mean "it doesn't run" ? Is the device in reset, is the code in some exception? Or it is stuck waiting for some conditions?
best regards,
Peter
Hello,
I used the "LWIP" project in the example,I compiled this project into "Flash". When I reset the device, There is no network transmission. (The way I think it is that after compiling into Flash, the project should be able to work ,whenever open the power supply.)
And I think it has a condition, because every time I compile, I need to press "resume" twice( Usually I think just press "resume" once. )
When I first hit "resume", it looked like this:
It didn't work until I hit "resume" a second time.
I want to know what should I do to make it work every time I turn on the power.
best regards,
Li Xu