The TIM filter mode of 5777M

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The TIM filter mode of 5777M

Jump to solution
448 Views
Jamber_H
Contributor III

Hi, 

I have some question about the filter mode of TIM.

1. The up/down counter mode with rising edge, after F_OUT reaches High level, does the FLT_CNT decremented?

Up_Down_Counter.bmp

2. The Hold counter mode with rising edge, after F_OUT reaches High level, how does the FLT_CNT reset? If the cnt can't be reset, does it means the filter only can work one time?

Hold_Counter.bmp

Best Regards

Jamber

Tags (3)
0 Kudos
1 Solution
432 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

1) I think functionality clearly follows following statement.

davidtosenovjan_0-1670237886252.png

2) I seems to be shown in mixed mode description where detection of falling edge is apparently in de-glitch counter propagation mode with hold counter and reset after F_OUT is set.

davidtosenovjan_1-1670238202761.png

 

 

View solution in original post

0 Kudos
2 Replies
433 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

1) I think functionality clearly follows following statement.

davidtosenovjan_0-1670237886252.png

2) I seems to be shown in mixed mode description where detection of falling edge is apparently in de-glitch counter propagation mode with hold counter and reset after F_OUT is set.

davidtosenovjan_1-1670238202761.png

 

 

0 Kudos
429 Views
Jamber_H
Contributor III

Hi, David

Thank you for your reply, I see the description and fig in usermanual. 

The falling edge shown in Figure 10-7 is filtered with up/down counter mode. The moment of you marked in red box, after the FLT_CNT reaches FLT_FE, the FLT_CNT reset to 0. I can't find any explicit description about this behaior in UserManual,  and it is contradictory with Figure 10-5.

According to Figure 10-7, Figure10-5 should be like this:

UpDown_C.bmp

and Figure 10-6 should be like this:

Hold_C.bmp

Is my description right?

Best Regards

Jamber

0 Kudos