The DMA's end-of-major loop interrupt keeps getting triggered

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The DMA's end-of-major loop interrupt keeps getting triggered

844 Views
ybb34713
Contributor II
   I used PWM-CTU-ADC-DMA patterns in developing motor controls based on MPC5741P, and DMA's end-of-major loop interrupt(INTMAJOR) is enabled. Now the question is that
  1. CTU has the right trigger frequency, but ISR is triggered again just after it has run, and it's going to keep doing that.
  2. TCDn CSR[DONE] flag bit cannot be cleared by writing 1 to DMA_CDNE[CADN].

DMA Channel 0 init:

void DMA_Channel_Config(u8 DAM_channel,u32 src,u32 dst)
{
    DMA_0.ERQ.B.ERQ0 = 0;    //The DMA request signal for channel 0


    DMA_0.TCD[DAM_channel].SADDR.R = src;
    DMA_0.TCD[DAM_channel].SOFF.R = 0;
    DMA_0.TCD[DAM_channel].SLAST.R = 0;
    DMA_0.TCD[DAM_channel].ATTR.B.SMOD = 0;
    DMA_0.TCD[DAM_channel].ATTR.B.SSIZE = 1;


    DMA_0.TCD[DAM_channel].DADDR.R = dst;
    DMA_0.TCD[DAM_channel].DOFF.R = 2;
    DMA_0.TCD[DAM_channel].DLASTSGA.R = -16;
    DMA_0.TCD[DAM_channel].ATTR.B.DMOD = 0;
    DMA_0.TCD[DAM_channel].ATTR.B.DSIZE = 1;

    DMA_0.TCD[DAM_channel].CSR.B.DREQ = 0;  /*The channel’s ERQ bit is not affected*/
    DMA_0.TCD[DAM_channel].NBYTES.MLNO.B.NBYTES = 16;

    DMA_0.TCD[DAM_channel].BITER.ELINKNO.B.ELINK = 0;     
    DMA_0.TCD[DAM_channel].BITER.ELINKNO.B.BITER = 1;
    DMA_0.TCD[DAM_channel].CITER.ELINKNO.B.ELINK = 0;      
    DMA_0.TCD[DAM_channel].CITER.ELINKNO.B.CITER = 1;

    DMA_0.TCD[DAM_channel].CSR.B.INTHALF = 0;     /* No interrupt when major count half complete */
    DMA_0.TCD[DAM_channel].CSR.B.INTMAJOR = 1;    /*interrupt when major count completes */
    DMA_0.TCD[DAM_channel].CSR.B.MAJORELINK = 0;  /* Dynamic program is not used */
    DMA_0.TCD[DAM_channel].CSR.B.MAJORLINKCH = 0; /* No link channel # used */
    DMA_0.TCD[DAM_channel].CSR.B.ESG = 0;         /* Scatter Gather not Enabled */
    DMA_0.TCD[DAM_channel].CSR.B.BWC = 0;         /* Default bandwidth control- no stalls */
    DMA_0.TCD[DAM_channel].CSR.B.START = 0;       /* Initialize status flags START, DONE, ACTIVE */
    DMA_0.TCD[DAM_channel].CSR.B.DONE = 0;
    DMA_0.TCD[DAM_channel].CSR.B.ACTIVE = 0;

    DMA_0.ERQ.B.ERQ0 = 0x1;    //The DMA request signal for channel 0
}

The location of the ISR in the intc_SW_mode_isr_vectors_MPC5744P.c:

        (uint32_t) &dummy, /* Vector #  50 Reserved for Platform periodic timer 3_2 (STM) */
        (uint32_t) &dummy, /* Vector #  51 Reserved for Platform periodic timer 3_3(STM) */
        (uint32_t) &dummy, /* Vector #  52 eDMA Combined Error eDMA */
        (uint32_t) &HW_eDMA_Channel0_ISR, /* Vector #  53 eDMA Channel 0 eDMA */
        (uint32_t) &dummy, /* Vector #  54 eDMA Channel 1 eDMA */
        (uint32_t) &dummy, /* Vector #  55 eDMA Channel 2 eDMA */
        (uint32_t) &dummy, /* Vector #  56 eDMA Channel 3 eDMA */

 

 

Tags (1)
0 Kudos
3 Replies

776 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi,

how the ISR looks like? Do you clear interrupt flag within ISR?

0 Kudos

776 Views
ybb34713
Contributor II

   Yeah, I cleared interrupt flag by DMA_0.CDNE.B.CADN = 1. Need I to clear other interrupt flag?

 

0 Kudos

776 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Use DMA_INT or DMA_CINT register.

0 Kudos