关于TJA1040数据传输问题,最近我们在应用中发现一块板子的CAN收发器(TJA1040)在与另一块电路板通信时无法发送和接受任何CAN数据(对方使用的是具有CAN总线唤醒的CAN收发器),当对方收发器已经处于唤醒状态下,双方通信正常,当对方处于待唤醒状态时,无论我们单片机如何给收发器发数据,均无数据输出来唤醒对方。然后换了一块相同的板子(同样使用TJA1040)再跟对方通信,此时没有任何问题,可以发出数据唤醒对方,并正常通信。请问这种情况是由于什么原因导致的,TJA1040有没有这种失效的可能性?