Some possible bugs in S32_SDK_MPC574xx_RTM_1.0.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Some possible bugs in S32_SDK_MPC574xx_RTM_1.0.0

ソリューションへジャンプ
539件の閲覧回数
shanix
Contributor II

Hello

When I use the S32_SDK_MPC574xx_RTM_1.0.0 on the MPC5748G, I found some code in SDK that may be problematical and would like to have it confirmed. Thanks.

shanix_0-1694400455999.pngshanix_1-1694400463453.png

 

 

0 件の賞賛
1 解決策
482件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

you have quite old SDK version, I can recommend to use the latest one, below is snippet from RTM 3.0.3

 

2023-09-11_12-13-32.png

Yes, setting of WRNEN is possible in Freeze mode only. 
A driver enable error interrupts if you install error callback using FLEXCAN_DRV_InstallErrorCallback, and Freeze mode is entered in it.

BR, Petr

元の投稿で解決策を見る

0 件の賞賛
3 返答(返信)
483件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

you have quite old SDK version, I can recommend to use the latest one, below is snippet from RTM 3.0.3

 

2023-09-11_12-13-32.png

Yes, setting of WRNEN is possible in Freeze mode only. 
A driver enable error interrupts if you install error callback using FLEXCAN_DRV_InstallErrorCallback, and Freeze mode is entered in it.

BR, Petr

0 件の賞賛
479件の閲覧回数
shanix
Contributor II
Thanks! Your reply is very useful. Maybe I need to migrate to the new verison SDK.
0 件の賞賛
506件の閲覧回数
shanix
Contributor II

shanix_0-1694419453801.png

 

0 件の賞賛