SPT tool fails to install

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SPT tool fails to install

1,047件の閲覧回数
adrianonea
Contributor III

I tried to install the software from the following link:

It fails to install and the messages asks me to login as administrator. I am actually logged in as administrator on a Win7 system. The name is not Administrator though. I can not create an account with "Administrator" name. 
ラベル(1)
タグ(1)
5 返答(返信)

779件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hi,

I tried to install SPT Tool into Win7 with account which is in Administrators group (account does not have administrator in it's name) and it works correct. Could you please try to install SPT Tool to different computer? It seems there is some problem in your operating system.

Could you please post here the screen of the installation error?

Regards,

Martin

778件の閲覧回数
adrianonea
Contributor III

Thank you Martin,I solved the problem by ticking the "Run This Program as an Administrator" checkbox from the Right Click-> Properties->Compatibility Tab. Attached is the snip.However this does not solve my problem. I was after a tutorial/user guide/step by step example on how to use the SPT, the Graph functionality from D32DS and integrate it with a c/c++ program.The processor I use is S32DS but I assume the SPT is the same with MPC5775k.

From: b55689 <admin@community.nxp.com>

To: adrian onea <adrian_onea@yahoo.com>

Sent: Tuesday, 27 December 2016, 19:54

Subject: Re: - Re: SPT tool fails to install

#yiv8690589555 * #yiv8690589555 a #yiv8690589555 body {font-family:Helvetica, Arial, sans-serif;}#yiv8690589555 #yiv8690589555 h1, #yiv8690589555 h2, #yiv8690589555 h3, #yiv8690589555 h4, #yiv8690589555 h5, #yiv8690589555 h6, #yiv8690589555 p, #yiv8690589555 hr {}#yiv8690589555 .yiv8690589555button td {}

|

NXP Community

|

Re: SPT tool fails to install

reply from Martin Kovar in MPC5xxx - View the full discussionHi, I tried to install SPT Tool into Win7 with account which is in Administrators group (account does not have administrator in it's name) and it works correct. Could you please try to install SPT Tool to different computer? It seems there is some problem in your operating system. Could you please post here the screen of the installation error? Regards,Martin

Reply to this message by replying to this email, or go to the message on NXP Community

Start a new discussion in MPC5xxx by email or at NXP Community

Following Re: SPT tool fails to install in these streams: Inbox

This email was sent by NXP Community because you are a registered user.

You may unsubscribe instantly from NXP Community, or adjust email frequency in your email preferences |

|

0 件の賞賛

779件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hi,

I am not sure if I understand correct. Do you want some guide for SPT Graphical Tool included in S32 Design Studio? If yes, please open S32 Design Studio installation folder and go to the following path:

S32_Power_v1.1\S32DS\help\pdf\s32ds.pwr.win.gt_reference_manual.pdf

If no, please clarify me your requirement more detail.

Regards,

Martin

779件の閲覧回数
adrianonea
Contributor III

Yes, I want some guide on how to use the SPT graphical tool. I have already red the pdf but:It only discusses the ide very briefly. It does not say what else do you have to do to interact between the generated .spt and the rest of the program.Do we have to add anything manually to any of the memory maps or other config files? labels/sections/ assembler directives etc.

Also I can't open the "properties" page for one instruction.

There is an update "update 1" for S32DS listed on your web page but when I follow the link it is not available.

I have the 1.1 power PC version for windows from June 2016.

From: b55689 <admin@community.nxp.com>

To: adrian onea <adrian_onea@yahoo.com>

Sent: Wednesday, 28 December 2016, 19:07

Subject: Re: - Re: SPT tool fails to install

#yiv4909912961 * #yiv4909912961 a #yiv4909912961 body {font-family:Helvetica, Arial, sans-serif;}#yiv4909912961 #yiv4909912961 h1, #yiv4909912961 h2, #yiv4909912961 h3, #yiv4909912961 h4, #yiv4909912961 h5, #yiv4909912961 h6, #yiv4909912961 p, #yiv4909912961 hr {}#yiv4909912961 .yiv4909912961button td {}

|

NXP Community

|

Re: SPT tool fails to install

reply from Martin Kovar in MPC5xxx - View the full discussionHi, I am not sure if I understand correct. Do you want some guide for SPT Graphical Tool included in S32 Design Studio? If yes, please open S32 Design Studio installation folder and go to the following path:S32_Power_v1.1\S32DS\help\pdf\s32ds.pwr.win.gt_reference_manual.pdf If no, please clarify me your requirement more detail. Regards,Martin

Reply to this message by replying to this email, or go to the message on NXP Community

Start a new discussion in MPC5xxx by email or at NXP Community

Following Re: SPT tool fails to install in these streams: Inbox

This email was sent by NXP Community because you are a registered user.

You may unsubscribe instantly from NXP Community, or adjust email frequency in your email preferences |

|

0 件の賞賛

778件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hi,

unfortunately, there is not any other manual to SPT graphical tool. There is only the one, which is part of S32DS installation.

I checked the link on web page and it does not work. Please try to download update1 directly from website. Click S32 Design Studio for power and on the next screen you will find the update.

S32 Design Studio IDE|NXP 

Regards,

Martin