S32 Design Studio for PowerPC Licensing and GCC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32 Design Studio for PowerPC Licensing and GCC

ソリューションへジャンプ
1,396件の閲覧回数
michaelgoudey
NXP Employee
NXP Employee


I have installed S32DS for ARM and also have taken a look at pre-release PPC version.  Where is the license file included with this installation?  It's not at all obvious like the directory structure included with KDS.

 

I would also like to know about GCC version included with S32DS for PowerPC.  It appears to be a VLE toolchain with GCC v4.9.2.  The one included with S32DS for ARM looks like GCC v4.9.3.

 

Is the VLE toolchain a custom one, or standard GCC?  I have searched the web and it's unclear whether VLE was added to the standard GCC compiler.

 

Thanks, Michael

ラベル(1)
1 解決策
747件の閲覧回数
stanish
NXP Employee
NXP Employee

Hello Michael,

Actually S32DS for ARM/Power v1.0 does not require any specific license file.

S32DS Basic framework is based on GNU components (GCC, GDB, Eclipse...) similarly as e.g. KDS.

Regarding S32DS for Power - it indeed includes VLE toolchain. VLE support has been added by Freescale into standard GCC (4.9.2)

Hope it helps.

Stanislav

元の投稿で解決策を見る

2 返答(返信)
748件の閲覧回数
stanish
NXP Employee
NXP Employee

Hello Michael,

Actually S32DS for ARM/Power v1.0 does not require any specific license file.

S32DS Basic framework is based on GNU components (GCC, GDB, Eclipse...) similarly as e.g. KDS.

Regarding S32DS for Power - it indeed includes VLE toolchain. VLE support has been added by Freescale into standard GCC (4.9.2)

Hope it helps.

Stanislav

747件の閲覧回数
michaelgoudey
NXP Employee
NXP Employee

Thanks Stanislav.

This is exactly what I was looking for.  S32DS does not use a custom toolchain, and VLE has been added to standard GCC.  Can I see the support in a GCC git tree somewhere?

Regards,


Michael Goudey

0 件の賞賛