Question About MAC57D5xx

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Question About MAC57D5xx

432 次查看
alighieri
Contributor III

HELLO

We're Considering MAC57D5xx For Instrument Cluster Integrated With Head Unit. First We Need Video Over Video Feature Which Will Need Overlay 2 Input Video / OSD Upon Video In Resolution 1920*1080P. I See Reference Manual Says Then Datasheet Says Supports 2 x WVGA Displays WVGA Mean Resolution Lower Then 1024*800. And From Reference Manual / Datasheet Here Is No Definite Specification About Frame Rate Support Up To. Can You Help To Confirm My Questions

pastedImage_1.png

We Need To Inverse The Horizontal And Vertical For Portrait 12.1 Inch Display. As Mentioned We Want To Design Cluster / Infotainment Device Integration MAC57D5xx Will Be Used For Display Control. Can MAC57D5xx  Support Invert H Total To V Total To Rotate Display?

About Layer. What Is The Purpose Layers Of 2D-ACE Designed For? Can We Use That For Picture Over Picture / Picture In Picture?

Is Here Standalone Debug Interface For M4 / A5 / M0? How Can We Port OS (RTOS) / Firmware To Each Of Codes? How Can They Communicate With Each Others?

Do You Have 2D-ACE Register Table Or Initiation Use Sample Codes To Be Added Upon OS / Firmware?

Thanks 

0 项奖励
0 回复数