On the ADC conversion problem of MPC5744P

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

On the ADC conversion problem of MPC5744P

472 Views
boshimao
Contributor II

Hi,

I use the 144-pin MCU. There are now 22 channels that need to be converted using ADC0 (11 channels) and ADC1 (11 channels), which divide the 22 channels into two sections, the first four channels need to be converted once per PWM cycle (100us), and the second Some 18 channels require a 500ms conversion. I want to use CTU mode while the request is not lost. Please give suggestions.

Labels (1)
0 Kudos
0 Replies