When I use the sample project, the error log shows the following statement, " [!ERROR!]
"AUTOSAR release major version number of the Basic Software Module Description file (Gpt.epd version [!"ArReleaseMajorVersion "!]) and the Code template file (Gpt_PBcfg.c version [!"num:i($GPT_AR_RELEASE_MAJOR_VERSION_TEMPLATE)"!]) are different"
However, the two version numbers are same. 4.0.3
Hello,
It looks like the example is not matching the ASR 4.0
Could you share with me the Gpt_PBcfg.c version?
Best regards,
Peter