Hi,
Specifically for the MPC5746C
I am having some issues with setting the RUN_PC and LP_PC Configuration Registers.
I am trying to use PC7 and LP7 configurations for LIN1. When I try to enter initialization, it fails with "Error : Error in ONCE status register during instruction execution."
I know the problem is with RUN_PC[0]. If the modes for PC0 are enabled, then it works fine, but I should be setting the PC7 and LP7 for LIN1. I don't understand what the problem is.
Thank you,
解決済! 解決策の投稿を見る。
Hi,
it looks like it is caused by DBG_F bit in PCTL51 register. If you configure this bit as '0', is it working?
Regards,
Lukas
Hi,
it looks like it is caused by DBG_F bit in PCTL51 register. If you configure this bit as '0', is it working?
Regards,
Lukas
That was the problem. Thank you