MPC5777C: REACM used for simple output disable

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC5777C: REACM used for simple output disable

648 次查看
EAlepins
Contributor V

We would like to know if MPC5777C's REACM module can be used in a very simple manner:

- When ADC samples go over a limit, the output pin is permanently disabled (... until SW reconfigures the REACM channel)

I only saw periodic operation (PWMs). Is static operation also possible?

Also, is it possible to confirm threshold exceeding before taking an action on the output pin?

If all this is not possible, am I using the right MPC5777C module to do that job?

Thanks,

Étienne

标记 (2)
0 项奖励
回复
3 回复数

482 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, is this still an issue for you?

0 项奖励
回复

482 次查看
EAlepins
Contributor V

Yes, kind of. For now, since I had no answer, I have considered it is not possible, so we plan to do that job with an FPGA. But if you find a way to do it with the MPC5777C, it might be interesting.

Thanks,

Étienne

0 项奖励
回复

482 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

OK.

I do really think it is not possible with reaction module.

Maybe 'eTPU output disable feature' with conjunction with SDADC could be used for that, if I understood correctly what you are trying to achieve.

pastedImage_8.png

0 项奖励
回复