MPC5777C EBI chip select generation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5777C EBI chip select generation

Jump to solution
2,710 Views
NAIDU
Contributor III

Hi,

 I configured EBI with the following setting but CS is not generating 

1.PLL0 --- 192MHZ,PLL1-- 264MHZ

2.SYSCLKSEL -- PLL1,plat_clk = 132MHZ

3.clkout=66MHZ,engclk= 132/32

4.EBI configuration for 16 bit,non-multiplexed,CS access

EBI_MCR = 1;
EBI.BMCR.R = 0;
/*CS0 0x2000_0000–0x3FFF_FFFF*/

EBI.CAL[0].OR.R = 0;//(0xFFF00000);
EBI.CAL[0].OR.B.SCY = 0x0a;
EBI.CAL[0].BR.R = (0x20000000 | 0x1A2B);
SIU.PCR[256].R = 0x060F;//0x060F; CS0 config
SIU.PCR[294].R = 0x060F;//0x060F; RD_WR
SIU.PCR[277].R = 0x060F;//0x060F;

for (i=259;i<=277;i++)//address bus

{

 PCR[i] = 0x0440;

}

for (i=278;i<=293;i++)//data bus

{

 PCR[i] = 0x0440;

}

/*writing in external space in while*/

for(;;)

{

*(int *)(0x20000000) = 0x5555;

//delay

}

I am monitoring CS in oscilloscope,but it is not cumming. i am testing this on NXP EVB and project is created in S32DS.

please give some solution.

Thanks&Regards,

Naidu

0 Kudos
1 Solution
1,882 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

I am attaching test code I have written. It partially works on my side, but I have some preliminary version of MPC5777C-516DS where there is incorrectly routed D_ADD_DAT31 lines thus my simple test don't pass. But I can see in the debugger window it works, but data are slightly corrupted.

Please, let me know if it works on you side, hoping you have newer EVB. Thanks

View solution in original post

0 Kudos
13 Replies
1,882 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, do you have configured following jumper?

pastedImage_1.png

0 Kudos
1,882 Views
NAIDU
Contributor III

Hi David,

  I am checking pin 1 status in oscilloscope,it is not toggling,it is always high. Please see some more observations 

1.TLB entry in startup code for MMU initialisation and AN5191 are not matching.(table numbers)

2.in startup code RPN of external memory is zero,i changed it to 0x2000 but still it is not working. in metroworks for MPC5567 project, in HW_init function,for external memory  initialisation RPN and EPN are having same value.(0x2000)

3.In MPC5567 project with metroworks,external memory initialisation will happen only after the macro definition.here also we need to do any setting?

     If you are having any facility to check this problem in your lab then i will share entire project. Otherwise share the EBI firmware already tested is available with you.

Thanking You.

Regards,

Naidu

0 Kudos
1,882 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

I will share example code, probably tomorrow.

0 Kudos
1,882 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

You have incorrectly defined OR register that probably the reason why you don't see asserted chip-select.

See following document, section 5:

https://community.nxp.com/docs/DOC-101725 

0 Kudos
1,882 Views
NAIDU
Contributor III

I referred the section 5 of the document,OR value zero means entire memory space is selected,ia it correct? Anyway I checked with both OR values still it is not coming. Ok please share the software with CS access.  

0 Kudos
1,883 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

I am attaching test code I have written. It partially works on my side, but I have some preliminary version of MPC5777C-516DS where there is incorrectly routed D_ADD_DAT31 lines thus my simple test don't pass. But I can see in the debugger window it works, but data are slightly corrupted.

Please, let me know if it works on you side, hoping you have newer EVB. Thanks

0 Kudos
1,882 Views
NAIDU
Contributor III

Following is the MMU initialization in my project(which is generated by IDE)

e_lis r3, 0x1001
mtspr 624, r3

e_lis r4, 0xC000
e_or2i r4, 0x0480
mtspr 625, r4

e_lis r5, 0x4000
e_or2i r5, 0x0028
mtspr 626, r5

e_lis r6, 0x4000
e_or2i r6, 0x003f
mtspr 627, r6

tlbwe

e_lis r3, 0x1000
mtspr 624, r3

e_lis r4, 0xC000
e_or2i r4, 0x0700
mtspr 625, r4

e_lis r5, 0x0000
e_or2i r5, 0x0020
mtspr 626, r5

e_lis r6,0x0000
e_or2i r6, 0x003f
mtspr 627, r6

tlbwe

e_lis r3, 0x1002
mtspr 624, r3

e_lis r4, 0xC000
e_or2i r4, 0x0580
mtspr 625, r4

e_lis r5, 0xFFE0
e_or2i r5, 0x002A
mtspr 626, r5

e_lis r6, 0xFFE0
e_or2i r6, 0x003f
mtspr 627, r6

tlbwe

e_lis r3, 0x1003
mtspr 624, r3

e_lis r4, 0xC000
e_or2i r4, 0x0700
mtspr 625, r4

e_lis r5, 0x2000
e_or2i r5, 0x0020
mtspr 626, r5

e_lis r6,0x0000
e_or2i r6, 0x003f
mtspr 627, r6

tlbwe

e_lis r3, 0x1004
mtspr 624, r3

e_lis r4, 0xC000
e_or2i r4, 0x0580
mtspr 625, r4

e_lis r5, 0xC3E0
e_or2i r5, 0x002A
mtspr 626, r5

e_lis r6, 0xC3E0
e_or2i r6, 0x003f
mtspr 627, r6

tlbwe

In the given SW in External_SRAM_MMU_init() function you are refering TLB 2?is it ok?in above startup code it is at TLB3.

0 Kudos
1,882 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Yes, my startup uses TLB2 for external bus

#TLB2 = external bus @ 0x2000_0000, VLE
    e_lis   r3,0x1002
    mtspr   mas0,r3
    e_lis   r3,0xC000
    e_or2i  r3,0x0700
    mtspr   mas1,r3
    e_lis   r3,0x2000
    e_or2i  r3,0x0020
    mtspr   mas2,r3
    e_lis   r3,0x0000
    e_or2i  r3,0x003F
    mtspr   mas3,r3
    tlbwe

Feel free to modify it according your setup - btw following configurator could be possibly helpful for you:

https://community.nxp.com/docs/DOC-331924 

0 Kudos
1,882 Views
NAIDU
Contributor III

Hi,

   Thank you for quick support.

 1.what is the IDE you are using?i am unable to open the SW shared by you?

i try to do the changes as per shared SW in S32DS,but it is not accepting assembly instructions in .c file. 

 2.if possible share the SW with S32DS IDE.

Thanks&Regards,

Naidu

0 Kudos
1,882 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

It is based on GreenHills compiler. However all necessary setting regarding EBI is present in main.c file. It should not be difficult to port it into S32.

0 Kudos
1,882 Views
NAIDU
Contributor III

i am unable to add External_SRAM_MMU_init() function in my IDE,it contains TLB entry modification in assembly language and my compiler is giving error.

0 Kudos
1,882 Views
NAIDU
Contributor III

Hi david,

Thank you for your support,i added assembly instructions for TLB modification.now chip select is generating.

0 Kudos
1,882 Views
NAIDU
Contributor III

Can you please guide me how to open it through S32DS

0 Kudos