MPC5744P cancasexl bootloader

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5744P cancasexl bootloader

1,448件の閲覧回数
johnjiang888888
Contributor I

NXP MPC5744P

rbf: MPC5744P_S32DS_UART1_CAN0.rbf

tools:cancasexl+RAppID

description:The program can be loaded successfully,But it doesn't work,Why?

ラベル(1)
タグ(1)
0 件の賞賛
返信
4 返答(返信)

1,317件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

did you follow these instructions in the user manual?

pastedImage_1.png

And this is from the release notes:

pastedImage_2.png

This is the most common reason. The application will not work if the steps above are not implemented.

Regards,

Lukas

0 件の賞賛
返信

1,317件の閲覧回数
johnjiang888888
Contributor I

09C34E46-A636-40e5-A649-E835C97A0507.png

hello,where is my problem?

thanks

0 件の賞賛
返信

1,317件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

it's not about the settings of Rappid tool or about the RBF file. It's about the application which you are going to download by the bootloader. You need to implement the steps mentioned above.

Regards,

Lukas

0 件の賞賛
返信

1,317件の閲覧回数
johnjiang888888
Contributor I

Problem has been solved,Thank you

0 件の賞賛
返信