MPC5744P cancasexl bootloader

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5744P cancasexl bootloader

1,354 Views
johnjiang888888
Contributor I

NXP MPC5744P

rbf: MPC5744P_S32DS_UART1_CAN0.rbf

tools:cancasexl+RAppID

description:The program can be loaded successfully,But it doesn't work,Why?

Labels (1)
Tags (1)
0 Kudos
Reply
4 Replies

1,223 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

did you follow these instructions in the user manual?

pastedImage_1.png

And this is from the release notes:

pastedImage_2.png

This is the most common reason. The application will not work if the steps above are not implemented.

Regards,

Lukas

0 Kudos
Reply

1,223 Views
johnjiang888888
Contributor I

09C34E46-A636-40e5-A649-E835C97A0507.png

hello,where is my problem?

thanks

0 Kudos
Reply

1,223 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

it's not about the settings of Rappid tool or about the RBF file. It's about the application which you are going to download by the bootloader. You need to implement the steps mentioned above.

Regards,

Lukas

0 Kudos
Reply

1,223 Views
johnjiang888888
Contributor I

Problem has been solved,Thank you

0 Kudos
Reply