MPC5744 SENT driver compilation failed

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MPC5744 SENT driver compilation failed

跳至解决方案
1,032 次查看
gsr007
Contributor I

 Dear expert:  

    At S32DS,I tried  to run the SENT driver in AN4856 for 5744. But there are many compilation errors.

gsr007_1-1694488220470.pnggsr007_2-1694488245137.pnggsr007_3-1694488256740.pnggsr007_4-1694488265180.png

So,my questions include these points:

1.what is the root cause of the above problems? Are there errors in my project configuration?But I have run other drivers successfully before,for example the ADC driver,the CAN driver and so on.

2.How to solve these problems?

Also, I saw that someone had asked a similar question, but it was not resolved in the end.

Thanks.

 
0 项奖励
1 解答
1,006 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

that driver/example was done in GreenHills so importing to teh S32DS could not be such easy and you need to do it yourself.
Anyway, there is SDK demo example for SENT receiver within S32DS, so you can refer to it;
c:\NXP\S32DS_Power_v2.1\S32DS\software\S32_SDK_S32PA_RTM_3.0.3\examples\MPC5744P\driver_examples\communication\srx_fast_dma\Doxygen\srx_fast_dma_mpc5744p.dox

BR, Petr

在原帖中查看解决方案

0 项奖励
4 回复数
1,007 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

that driver/example was done in GreenHills so importing to teh S32DS could not be such easy and you need to do it yourself.
Anyway, there is SDK demo example for SENT receiver within S32DS, so you can refer to it;
c:\NXP\S32DS_Power_v2.1\S32DS\software\S32_SDK_S32PA_RTM_3.0.3\examples\MPC5744P\driver_examples\communication\srx_fast_dma\Doxygen\srx_fast_dma_mpc5744p.dox

BR, Petr

0 项奖励
964 次查看
gsr007
Contributor I

Thank you for your reply!

Also, I would like to know where to obtain this document?

Thanks!

0 项奖励
941 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

it is just very short description of the demo example. So install SDK and you can locate it there.

BR, Petr

0 项奖励
939 次查看
gsr007
Contributor I

Your replies are ver helpful to me.

Thank you very much.

0 项奖励