MPC5606B startertrak board max input voltage for port pins

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5606B startertrak board max input voltage for port pins

ソリューションへジャンプ
1,791件の閲覧回数
sundar19
Contributor III

Hi,

I am using mpc5606b startertrak dev board . I have attached external transceivers TJA1050 with the CAN bus pins. I have supplied 5V to transceivers and thus the same logic voltage is applied to CAN port pins of mpc5606b. Can mpc5606b pins take 5V input? Will it damage the pins? 

0 件の賞賛
返信
1 解決策
1,776件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

TRK-MPC5606B is supplied by 5V only, it's not configurable to 3.3V. So, there's no problem, you can connect a transceiver supplied by 5V.

The microcontroller itself supports both 3.3V and 5V supply voltage.But if 3.3V is used, the GPIO pins are not 5V tolerant.

Regards,

Lukas

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
1,777件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

TRK-MPC5606B is supplied by 5V only, it's not configurable to 3.3V. So, there's no problem, you can connect a transceiver supplied by 5V.

The microcontroller itself supports both 3.3V and 5V supply voltage.But if 3.3V is used, the GPIO pins are not 5V tolerant.

Regards,

Lukas

0 件の賞賛
返信
1,769件の閲覧回数
sundar19
Contributor III

You saying that if I power up mpc5606b with 3.3V , then its pins arent 5V tolerant? 
thank you

0 件の賞賛
返信
1,763件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Yes, you can find in the datasheet:

lukaszadrapa_0-1621596721976.png

 

Regards,

Lukas

0 件の賞賛
返信
1,764件の閲覧回数
sundar19
Contributor III

Thank you

0 件の賞賛
返信
1,772件の閲覧回数
sundar19
Contributor III

Thank you so much

0 件の賞賛
返信