MPC5606B BAM Serial Communication

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5606B BAM Serial Communication

Jump to solution
831 Views
fscheidl
Contributor II

I just read about the included Boot Assist Module in MPC5606B. I understand that I have to set the FAB and ABS pins accordingly to disable booting from internal flash and make use of the Boot Assist Module instead.

 

Is the LINFlex_0 module set to UART mode automatically when I set the FAB and ABS pins accordingly?

Is it correct that I have to use the LINFlex_0 module in order to communicate with the MCU in BAM status?

For booting from CAN, I guess the relevant pins/module is FlexCAN_0 (CAN0TX, CAN0RX) then?

 

Thank you very much in advance!

Labels (1)
Tags (4)
0 Kudos
1 Solution
607 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

- Is the LINFlex_0 module set to UART mode automatically when I set the FAB and ABS pins accordingly?

- Yes.

- Is it correct that I have to use the LINFlex_0 module in order to communicate with the MCU in BAM status?

- Yes:

pastedImage_0.png

- For booting from CAN, I guess the relevant pins/module is FlexCAN_0 (CAN0TX, CAN0RX) then?

- Yes:

pastedImage_1.png

Regards,

Lukas

View solution in original post

1 Reply
608 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

- Is the LINFlex_0 module set to UART mode automatically when I set the FAB and ABS pins accordingly?

- Yes.

- Is it correct that I have to use the LINFlex_0 module in order to communicate with the MCU in BAM status?

- Yes:

pastedImage_0.png

- For booting from CAN, I guess the relevant pins/module is FlexCAN_0 (CAN0TX, CAN0RX) then?

- Yes:

pastedImage_1.png

Regards,

Lukas