Looking at MPC555 / MPC556 datasheet for I/O drive strength in page 64, a strength of 25/50pF is mentioned for 3V pins.
This is confusing because I cant confirm whether 25pF strength is for MPC555 and 50pF strength is for MPC556,
OR
25pF is half strength and 50pF is full strength for both MPC555/MPC556,
Can you please explain.
Thanks
已解决! 转到解答。
Hi,
the only difference between MPC555 and MPC556 is that MPC556 supports code compression. Other characteristics are exactly the same.
As you mentioned, 25/50pF means 25pF for reduced drive strength and 50pF for full drive strength.
Regards,
Lukas
Hi,
the only difference between MPC555 and MPC556 is that MPC556 supports code compression. Other characteristics are exactly the same.
As you mentioned, 25/50pF means 25pF for reduced drive strength and 50pF for full drive strength.
Regards,
Lukas