How to gain access to censored SPC560D30 via JTAG

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to gain access to censored SPC560D30 via JTAG

1,650 Views
ulbed
Contributor I

How can I access the device via JTAG? I have the censorship password. In Reference Manual there's only on note:

 

JTAG password details:

Enter password as
{NVPWD1, NVPWD0}

example –
0x89ABCDEF_01234567

 

But how and where should I enter it (register?) ?

Labels (1)
0 Kudos
Reply
4 Replies

1,125 Views
panrui
Contributor I
you should refer to:
Example MPC5604B Censorship CW210
link:The document included in this demo addresses this kind of censorship problem very well.
0 Kudos
Reply

1,125 Views
martin_kovar
NXP Employee
NXP Employee

Hi,

try the following process described in official Lauterbach documentation:

pastedImage_0.png

Regards,

Martin

0 Kudos
Reply

1,125 Views
ulbed
Contributor I

This is definiteIy not a solution. This process only describes Lauterbach specific configuration. Neither does It say what the Lauterbach debugger does, nor do I have one to test it. I am using my own developed debugger and I have to add the feature to access censored devices. So what I need is the description of JTAG censorship unlocking sequence. It is mentioned but not explained in the reference manual:

pastedImage_0.png

0 Kudos
Reply

1,125 Views
martin_kovar
NXP Employee
NXP Employee

Hi,

I would like to apologize for my misunderstanding.

Please look at the following app note, which should be more helpful for you.

http://cache.nxp.com/files/32bit/doc/app_note/AN4365.pdf?fsrch=1&sr=1&pageNum=1

Regards,

Martin

0 Kudos
Reply