Firmware Over-The-Air (FOTA) on MPC5748G

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Firmware Over-The-Air (FOTA) on MPC5748G

Jump to solution
2,218 Views
MattJCole
Contributor V

 

I would like to implement FOTA on the MPC5748G but I am not able to find out how to get started. I have found tons of information telling me what it is and how good it is but nothing about how to start using it on my processor. I still do not know if it is a boot loader or is it a library you compile with your operational code. can some one give me a link to where I can download what I need to get started? 

 

 

0 Kudos
1 Solution
2,127 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

in the mentioned AN5319, I added this asm code right to the beginning of __start:

;******************************************************************************
; Check if Bootloader or User Application is supposed to be executed
; Pin PA[1] is used. PA[1] signal is routed to SW3 on EVB board.
; If PA[1] == 0 - execute User Application
; If PA[1] == 1 - execute Bootloader

;configure pin PA[1] as input - write SIUL2.MSCR[1].R = 0x00080000
;load address of SIUL2.MSCR[1] to r12
e_lis r12,0xFFFC
e_or2i r12,0x0244

;load immediate value to r11 which will enable the buffer
e_lis r11,0x0008

;write the value to SIUL2.MSCR[1]
e_stw r11,0(r12)

;check if SW3 is pushed down - if SIUL.GPDI[1] == 0x01
;load address of SIUL.GPDI[1] to r12
e_lis r12,0xFFFC
e_or2i r12,0x1501

;read the SIUL.GPDI[1] register
e_lbz r0,0(r12)

;compare the values - is the SW1 pushed?
se_cmpli r0,0x01

;execute bootloader or user application
;if pushed,executed bootloader
e_beq bootloader

;otherwise jump to user application

;but first check, if there's valid boot header at address 0xF9_4000
;load address of boot header to r12
e_lis r12,0x00F9
e_or2i r12,0x4000

;load upper half of boot header word to r0
;(lower half is application dependent)
e_lhz r0,0(r12)

;boot header should be 0x005A
e_cmpl16i r0,0x005A

;if the boot header is not valid, execute bootloader
e_bne bootloader

;if the boot header is valid, execute application
;load address of reset vector to r12
e_lis r12,0x00F9
e_or2i r12,0x4010

;load reset vector to r0
e_lwz r0,0(r12)
;move reset vector to link register
mtlr r0
;branch to address in link register
se_blrl

;******************************************************************************
bootloader:
;******************************************************************************
; When bootloader is going to be executed, disable Software watchdog 0
; The watchdog is kept enabled if user application is executed.

;SWT_0.SR.R = 0xc520;
e_lis r12,0xFC05

...

This code can be found in file crt0.ppc.

When you want to jump to the application later in C code, you can use something like:

typedef void (*func_ptr)();

(*(func_ptr)ADDRESS_OF_ENTRY_POINT)();

If you do not jump to the application right after reset (like in the asm code above), it is a good practice to disable all interrupts before the jump (by MSR[EE], by local enable bits in peripherals, by priorities in INTC) and also deinit all used peripherals to default reset state.

Regards,

Lukas

View solution in original post

0 Kudos
9 Replies
2,106 Views
MattJCole
Contributor V

I am using the DEVKIT-MPC5748G

Trying to get the bootloader to work has caused to make negative progress. I am in a worse state know then I was before I I tried to get the bootloader run. I uses to be able to upload an application to flash and when I pressed the reset button the dev board run the application. How do i get back to at least that state. 

0 Kudos
2,143 Views
MattJCole
Contributor V

I think this is the last question and it should be a simple one. How do I load the application from the bootloader. I can not seem to find any example code on how to jump to the location in flash where the application is. 

0 Kudos
2,128 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

in the mentioned AN5319, I added this asm code right to the beginning of __start:

;******************************************************************************
; Check if Bootloader or User Application is supposed to be executed
; Pin PA[1] is used. PA[1] signal is routed to SW3 on EVB board.
; If PA[1] == 0 - execute User Application
; If PA[1] == 1 - execute Bootloader

;configure pin PA[1] as input - write SIUL2.MSCR[1].R = 0x00080000
;load address of SIUL2.MSCR[1] to r12
e_lis r12,0xFFFC
e_or2i r12,0x0244

;load immediate value to r11 which will enable the buffer
e_lis r11,0x0008

;write the value to SIUL2.MSCR[1]
e_stw r11,0(r12)

;check if SW3 is pushed down - if SIUL.GPDI[1] == 0x01
;load address of SIUL.GPDI[1] to r12
e_lis r12,0xFFFC
e_or2i r12,0x1501

;read the SIUL.GPDI[1] register
e_lbz r0,0(r12)

;compare the values - is the SW1 pushed?
se_cmpli r0,0x01

;execute bootloader or user application
;if pushed,executed bootloader
e_beq bootloader

;otherwise jump to user application

;but first check, if there's valid boot header at address 0xF9_4000
;load address of boot header to r12
e_lis r12,0x00F9
e_or2i r12,0x4000

;load upper half of boot header word to r0
;(lower half is application dependent)
e_lhz r0,0(r12)

;boot header should be 0x005A
e_cmpl16i r0,0x005A

;if the boot header is not valid, execute bootloader
e_bne bootloader

;if the boot header is valid, execute application
;load address of reset vector to r12
e_lis r12,0x00F9
e_or2i r12,0x4010

;load reset vector to r0
e_lwz r0,0(r12)
;move reset vector to link register
mtlr r0
;branch to address in link register
se_blrl

;******************************************************************************
bootloader:
;******************************************************************************
; When bootloader is going to be executed, disable Software watchdog 0
; The watchdog is kept enabled if user application is executed.

;SWT_0.SR.R = 0xc520;
e_lis r12,0xFC05

...

This code can be found in file crt0.ppc.

When you want to jump to the application later in C code, you can use something like:

typedef void (*func_ptr)();

(*(func_ptr)ADDRESS_OF_ENTRY_POINT)();

If you do not jump to the application right after reset (like in the asm code above), it is a good practice to disable all interrupts before the jump (by MSR[EE], by local enable bits in peripherals, by priorities in INTC) and also deinit all used peripherals to default reset state.

Regards,

Lukas

0 Kudos
2,174 Views
MattJCole
Contributor V

I kind figured that was the case. I just wanted to make sure.

0 Kudos
2,184 Views
MattJCole
Contributor V

I noticed the example is for the S32K144 and S32K146. Is there an example for the MPC5748G family?

0 Kudos
2,176 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Unfortunately no. There's only mentioned AN5319.

0 Kudos
2,186 Views
MattJCole
Contributor V

There is a lot of information to go over and it will take some time to go over but I think this is what I need.

0 Kudos
2,193 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hello Matt,

you can find a lot of documents to read here:

https://www.google.com/search?client=firefox-b-d&q=MPC5748G+AND+OTA+site%3Acommunity.nxp.com

To have some examples for the beginning:

Simple serial bootloader for MPC5748G:

https://www.nxp.com/docs/en/application-note/AN5319.pdf

https://www.nxp.com/docs/en/application-note-software/AN5319SW.zip

It does not implement a swap of applications, it only loads one application to the flash (always to the same area).

Then you can take a look at this application note written for S32K1 devices:

https://www.nxp.com/docs/en/application-note/AN12323.pdf

https://www.nxp.com/docs/en/application-note-software/AN12323SW.zip

Yes, it's different device but I believe it will be also helpful.

Regards,

Lukas

0 Kudos
2,195 Views
ZhouYiChuan
Contributor III

Generally, FOTA is a feature of the bootloader.
The new application flashing is started from a remote-server, not a technician beside your car.
So, if the flashing failed, the bootloader should roll-back to a correct application
And the Flash space in the processor should be sufficient for two copies of applicaton codes.

0 Kudos