DEVKIT-MPC5748G couldn't run after reset

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DEVKIT-MPC5748G couldn't run after reset

1,461 Views
ningwang
Contributor III

     Hi, I'm using DEVKIT-MPC5748G, and the hello+pll_z4_1 can run with on board open SDA with debug mode, and the led light. But if I press the  reset button, the program couldn't run from the internal flash.

     The linker file is attached.

     What's the reason?

     Thanks.

Original Attachment has been moved to: mem.ld.zip

Original Attachment has been moved to: libs.ld.zip

Original Attachment has been moved to: sections.ld.zip

0 Kudos
4 Replies

984 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

could you please specify, which version of S32DS you use? Could you please try to load the program and run it stand alone without debugger?

I tested on my side without debugger and it works correct.

Regards,

Martin

0 Kudos

984 Views
ningwang
Contributor III

Hi, Martin,

     Do you have the DEVKIT-5748G board and make a test of the example project "hello+pll_Z4_1" ?

Thanks a lot.

0 Kudos

984 Views
ningwang
Contributor III

Hi, Martin,

     Thanks for your reply. I'm using S32 Design Studio for Power Architecture, Version: 1.2 Build id: 170613

Linux version.

pastedImage_2.png

the console output:

Connection from "127.0.0.1" via 127.0.0.1
Copyright 2012 P&E Microcomputer Systems,Inc.
Command Line :/home/daniel/NXP/S32DS_Power_v1.2/eclipse/plugins/com.pemicro.debug.gdbjtag.ppc_1.6.7.201706090048/lin/pegdbserver_power_console -device=MPC5748G -startserver -singlesession -serverport=7224 -gdbmiport=6224 -interface=OPENSDA -speed=5000 -p
 
CMD>RE
 
Initializing.
MPC574xC Device detected.
Target has been RESET and is active.
CMD>CM /home/daniel/NXP/S32DS_Power_v1.2/eclipse/plugins/com.pemicro.debug.gdbjtag.ppc_1.6.7.201706090048/lin/gdi/P&E/nxp_mpc5748g_1x32x1524k_cflash.pcp
 
Initializing.
MPC574xC Device detected.
Initialized.
 
;version 1.04, 12/13/2016, Copyright P&E Microcomputer Systems, www.pemicro.com [5748G_6096k]
 
;device NXP, MPC5748G, 1x32x1524k, desc=CFlash
 
;begin_cs device=$00F8C000, length=$005F4000, ram=$40000000
 
Loading programming algorithm ...
 
WARNING - Selected .PCP file has been modified. CRC16 = $0869
Done.
CMD>VC
Verifying object file CRC-16 to device ranges ...
   block 00FA0000-00FA0007 ...
Calculated CRC-16 does not match block. (File = $0745, Device = $6820)
 
CMD>EM
 
Erasing.
Module has been erased.
CMD>PM
 
Programming.
Processing Object File Data ...
                                
                                
.
Programmed.
CMD>VC
Verifying object file CRC-16 to device ranges ...
   block 00FA0000-00FA0007 ...
Ok.
   block 00FA0010-00FA0017 ...
Ok.
   block 01000000-0100026D ...
Ok.
   block 01001000-010010F3 ...
Ok.
   block 01002000-01002BC7 ...
Ok.
   block 01002BD0-01002FDF ...
Ok.
   Checksum Verification Successful. (Cumulative CRC-16=$63DE)
 
CMD>RE
 
Initializing.
MPC574xC Device detected.
Target has been RESET and is active.
 
Starting reset script (/home/daniel/NXP/S32DS_Power_v1.2/eclipse/plugins/com.pemicro.debug.gdbjtag.ppc_1.6.7.201706090048/lin/gdi/P&E/s32e200_mpc574xg.mac) ...  
REM This script is compatible with MPC574xG devices.                                                                                                                                                     
REM Clean GPRs to remove residual data after using algorithm                                                                                                                                             
REM Initialize all of the Main SRAM - 768KB                                                                                                                                                              
Initializing RAM from $40000000 to $400BFFFF.
REM Core 0 I-MEM 16K                                                                                                                                                                                     
Initializing RAM from $50000000 to $50003FFF.
REM Core 0 D-MEM 64K                                                                                                                                                                                     
Initializing RAM from $50800000 to $5080FFFF.
REM Core 1 I-MEM 16K                                                                                                                                                                                     
Initializing RAM from $51000000 to $51003FFF.
REM Core 1 D-MEM 64K                                                                                                                                                                                     
Initializing RAM from $51800000 to $5180FFFF.
REM Core 2 I-MEM 16K                                                                                                                                                                                     
Initializing RAM from $52000000 to $52003FFF.
REM Core 2 D-MEM 32K                                                                                                                                                                                     
Initializing RAM from $52800000 to $52807FFF.
REM overlay memory 16K                                                                                                                                                                                   
Initializing RAM from $0D000000 to $0D003FFF.
REM Overlay SRAM Emulation device only                                                                                                                                                                   
Initializing RAM from $0C000000 to $0C0FFFFF.
 
Reset script (/home/daniel/NXP/S32DS_Power_v1.2/eclipse/plugins/com.pemicro.debug.gdbjtag.ppc_1.6.7.201706090048/lin/gdi/P&E/s32e200_mpc574xg.mac) completed.
 
MPC574xG Device detected.
No breakpoints currently set.
Disconnected from "127.0.0.1" via 127.0.0.1
Target Disconnected.
An unhandled exception occurred at $00007EFCBCC041A9:
EAccessViolation: Access violation
  $00007EFCBCC041A9
  $00007EFCBCC041DF
  $00007EFCBCC03C1E
  $00007EFCBDED37FE
  $00007EFCBDED3392
  $00007EFCBDED3528
  $00007EFCBDF1DE97
  $00007EFCBDEE96BB
  $00007EFCBDEDB5D7
  $00007EFCBDEEBA5C
  $00007EFCBDE5F411
  $00007EFCBDE5F4F9
  $000000000044DC71
  $0000000000401ED3

 

An unhandled exception occurred at $00007EFCBCC041A9:
EAccessViolation: Access violation
  $00007EFCBCC041A9
  $00007EFCBCC041DF
  $00007EFCBCC03B1D
  $00007EFCBDED37FE
  $00007EFCBDED3FE9
  $00007EFCBDE7F78E
  $00007EFCBF10B1FA

 

 

And still can't run after reset .  I also used the  Version: 1.2 Build id: 170613 windows version to test the demo "hello+pll_Z4_1", it's the same result. Still can not start after reset.

0 Kudos

848 Views
cricape06
Contributor I

Hi Ningwang,

Did you manage do fix this issue? I'm facing the same problem.

Thanks a lot.

0 Kudos