My PC's OS is windows 10. I installed tresos v24.0.0 tool.but it can't be loading when i open the tresos_gui.exe , with always stay in loading view.
And the window task manager shows his task"Java(TM) Platform SE binary" status is no response. when i closed the loading view,it show me the information like this(jdk-8u92-windows-i586 and jre-6u45-windows-i586 have been installed).
But Tresos v16.0.0 can loading his workspace normal.
Compared with tresos v16 and v24 's task status.
I have try to reinstall the tresos24 ,but the question can not be solved.
Thanks for your help.
解決済! 解決策の投稿を見る。
Hi,
Seems like there is an insufficient memory situation. You can try by increase maximum memory start of EB Tresos, by editing in tresos_gui.ini: -Xms256m => -Xms512m to see if the situation can be resolved. If it's not working, then maybe contacting Elektrobit support team directly is a better idea (https://www.elektrobit.com/support/)
Hi Nam,
I have the same problem with EB 25.1.1. Can you provide me hot-fix.
Best regards
Hi,
Since this topic is becoming harder to track, please create a ticket in support.nxp.com and we will support you via that portal.
Best Regards,
Nam
Hi Nam,
Thanks for quick answer.
New case under our project in support.nxp.com create.
Best regards
Hello,
I and facing the same issue, could I have to access to hot fix?
Thanks a lot.
Hello @_Hao_ ,
Could you share your account, so that I can ask internal team to grant the access?
Best Regards,
Nam
Thanks.
Could you share the link where I can download this hotfix?
BR
Hi, @namnguyenviet
I also facing the same problem with EB 24.0. Can you help to share the hotfix?
My email id is: fabio.marongiu@abinsula.com
Thanks in advance
Fabio
Hi, @namnguyenviet
I also facing the same problem with EB 26.0. Can you help to share the hotfix?
My email id is: chen.gilbert@inventec.com
thanks.
Hello @chen_gilbert ,
Your request has been processed. Please check in your SW licensing and Support.
Many thanks,
Nam
Hi,
I am also facing the same issue with EB version 26.0.0 where it is not able to launch the workspace and hangs at loading forever. I tried few approaches mentioned below:
1)Ending the Java task in Task Manager and try re launching the application.
2)Re installing the EB.
3) Replacing the dreisoft.tresos.launcher2.jar file
4)Restarting the PC .
But still the issue is not resolved and I get the error :
Workspace Cannot Be Locked: Could not launch the product because the associated workspace at 'C:\Vector\CBD1900941_D03_QF0\ThirdParty\Mcal_S32x\Supply\tresos\workspace' is currently in use by another Eclipse application.
Please specify another workspace with commandline argument "-data <path-to-workspace>".
when I try to generate EB Tresos Plugins from Davinci Configurator provided by Vector.
Please let me know how to resolve this issue.
Thanks & Regards,
Pooja
Hello @Pooja ,
Could you share with me your NXP account, which you have been used for register NXP products? We will share with you the EB hot-fix in order to see whether it can fix your issue.
Best Regards,
Nam
I need a fix for this. riglesias@borgwarner.com
@riglesias2021 , Which EB version you need the fix for?
a clarification of how to download the fix would be appreciated also. Thanks
24.0
@riglesias2021, Your access to hot-fix has granted.
Hello, the hotfix didnt solve my problem
SOLUTION: for me was just adding a "-clean" in the tresos_gui .ini