Excel MPC5777C clock configurator

キャンセル
次の結果を表示 
次の代わりに検索 
もしかして: 

Excel MPC5777C clock configurator

評価なし

Excel MPC5777C clock configurator

This config tool simplifies PLL setting calculation and clock configuration for MPC5777C device.

Version 1.3 added option to select between 264/300 MHz MCU versions.

               

Follow these steps

               

Note: Macros have to be enabled!

               

1. Enter frequency of used XOSC and desired PLL0 and PLL1 output.

     - put values into cells B14, Q13 and Q20 of the "Clocks" sheet

     - check if it is Valid or Invalid

     - "PLLconfig" sheet shows possible PLLs configurations                

 

2. Configure System and AUX clock selectors and its Dividers

     - check calculated frequency of System/Peripheral clocks

     - if Invalid change source clock and Divider value to keep Max freq

               

3. Copy generated code by pressing "Copy Code" button

ラベル(1)
タグ(3)
添付
バージョン履歴
最終更新日:
‎09-11-2020 03:45 AM
更新者: