Example MPC5674F TSENS-Temperature_calc CW210

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Example MPC5674F TSENS-Temperature_calc CW210

Example MPC5674F TSENS-Temperature_calc CW210

********************************************************************************
* Detailed Description:
* Example shows MCU's temperature measurement using internal temperature sensor.
* After basic initialization, the code initializes and calibrates eQADC, reads
* test flash content and performs all necessary ADC measurement to calculate die
* temperature. Results are then displayed in the terminal window.
* ------------------------------------------------------------------------------
* Test HW:         XPC567XKIT516 - MPC5674ADAT516 Rev.C, MPC567XEVBFXMB Rev.B
* MCU:             PPC5674FMVYA264
* Terminal:        19200-8-no parity-1 stop bit-no flow control on eSCI_A
* Fsys:            264/200/150/60 MHz
* Debugger:        Lauterbach Trace32
*                  PeMicro USB-ML-PPCNEXUS
* Target:          RAM, internal_FLASH
* EVB connection:  default
*
********************************************************************************

添付
評価なし
バージョン履歴
最終更新日:
‎04-11-2017 06:04 AM
更新者: