Example MPC5668G PinToggleStationery CW210

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Example MPC5668G PinToggleStationery CW210

No ratings

Example MPC5668G PinToggleStationery CW210

********************************************************************************

* Detailed Description:

* Application performs basic initialization, setup PLL to maximum allowed freq.,

* initializes interrupts, blinking one LED by interrupt, starts second core

* initializes and display notice via UART terminal and then terminals ECHO.

*

*

* Test HW:              MPC5688EVB

* MCU:                   SPC5668GMMG 0N61C

* Terminal:              19200-8-no parity-1 stop bit-no flow control on eSCI_A

* Fsys:                   116 MHz

* Debugger:             Lauterbach Trace32

*                             PeMicro USB-ML-PPCNEXUS

* Target:                  RAM, internal_FLASH

* EVB connection:   User LED 4 connected to pin P28-10

*

*

Labels (1)
Attachments
Version history
Last update:
‎12-29-2015 03:46 AM
Updated by: