mcxn236 usb device mode without VBUS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mcxn236 usb device mode without VBUS

ソリューションへジャンプ
554件の閲覧回数
allu
Contributor I

Hi NXP,

We refer NXP SDK_2_14_0_FRDM-MCXN236_rfp USB device example to develop a USB device. However, is it possible to make the USB device mode work without VBUS?

If yes, how can we modify this in the SDK?

Thanks,

Alan

ラベル(3)
0 件の賞賛
返信
1 解決策
489件の閲覧回数
diego_charles
NXP TechSupport
NXP TechSupport

Hi @allu 

Thank you very much for your patience.

As I reviewed internally, please find below our feedback. 

We strongly suggest customers to link MCX N2xx's USB_VBUS pin with USB connector as recommended in our  hardware design guide and  implemented in the official FRDM-MCX N 236 schematic.  

With the USB_VBUS pin detect, the application firmware can easily know  if the USB is attached or not.

Leaving USB_VBUS  floating is possible, but require the software  skip the attach detection, and use a software state machine to check if the USB is linked or not. But we are not sure about the workload to implement this.

Additonally, leaving USB_VBUS disconnect may impact on the USB certification attach and de-attach test, but it will not impact on other test items. As mentioned before, you may use the software approach to solve the attach and de-attach test item issue, but it is not our recommendation. 

Anyway, we strongly suggest you to enable the USB_VBUS.

Thank you, 

Diego

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
490件の閲覧回数
diego_charles
NXP TechSupport
NXP TechSupport

Hi @allu 

Thank you very much for your patience.

As I reviewed internally, please find below our feedback. 

We strongly suggest customers to link MCX N2xx's USB_VBUS pin with USB connector as recommended in our  hardware design guide and  implemented in the official FRDM-MCX N 236 schematic.  

With the USB_VBUS pin detect, the application firmware can easily know  if the USB is attached or not.

Leaving USB_VBUS  floating is possible, but require the software  skip the attach detection, and use a software state machine to check if the USB is linked or not. But we are not sure about the workload to implement this.

Additonally, leaving USB_VBUS disconnect may impact on the USB certification attach and de-attach test, but it will not impact on other test items. As mentioned before, you may use the software approach to solve the attach and de-attach test item issue, but it is not our recommendation. 

Anyway, we strongly suggest you to enable the USB_VBUS.

Thank you, 

Diego

0 件の賞賛
返信