I have RT1176 design that requires 2 different pinmux.c .h files for 2 projects that are 90% the same. I am certain it will require 2 projects. They are different at the hardware level. Is there a way in the build process to select 2 different pinmux.c .h files.
Hi @lfost
MCUXpresso can not add two pin_mux.c in one project.
I suggest that you can create two functions in the pin_mux.c, eg
BOARD_InitPins(void) BOARD_InitPins_1(void)
Hope this will help you.
Best regards,
Hang