Unable to detect IMXRT1170 eval board through USB/UART for MCUxpresso secure provisioning tool

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to detect IMXRT1170 eval board through USB/UART for MCUxpresso secure provisioning tool

180 Views
Jeevan
Contributor III

Hi Team,

I am using the MCUxpresso secure provisioning tool with IMXRT1170 eval board connected through the USB cable to the laptop.

But I am getting the below mentioned error when I run "Test connection". please help me resolve the issue as i am not able to write the image to the board using the tool.

Jeevan_0-1710238631316.png

 

0 Kudos
1 Reply

169 Views
marek-trmac
NXP Employee
NXP Employee

Hi Jeevan,

 

RT1170UART.jpg

SW1: ISP 0001, boot 0010;
for supply from USB: J38 3-4
for supply from UART: J38 7-8

For Octal Flash SW2-3 to 1

For OTFAD/IEE Encryption SW2-2 to 1

For SD CARD SW2-7 to 1

For SD CARD SW2-8 to 1

Regards,
Marek
0 Kudos