Unable to install SDK-2.3.1-MK22FX512Axxx12

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to install SDK-2.3.1-MK22FX512Axxx12

1,072 Views
divner
Contributor I

when will mcuxpresso support be available for the Kinetis SDK-2.3.1-MK22FX512Axxx12.

I am unable to drag N drop this SDK to install in MCuXpresso.

Thank you

0 Kudos
5 Replies

965 Views
nxf58474
NXP Employee
NXP Employee

Hi divner@hotmail.com,

 

Hope you are doing well. Which MCUXpresso version do you have? I downloaded the same SDK version and I was able to install it with no problem.

 

The SDK version requires MCUXpresso v10.0.x or later.

pastedImage_2.png

Hope this helps.

 

Best Regards,

Ricardo

0 Kudos

965 Views
divner
Contributor I

Noel Diviney Ayrenet Pty Ltd, Unit 3,80-88 Rodeo Drive, Dandenong South, Victoria 3175, Australia. Phone +61 413 120 892 email noel@ayrenet.com or divner@hotmail.com

0 Kudos

965 Views
divner
Contributor I

Hi Ricardo,

Thank you for your response.

I am using MCUXpresso V11.1.1.

There is no Dev Board for the MK22FX512AVLH12, so I had the SDK built for the device by following the instructions on the NXP Website. I am finding that this CPU seems to be the lone orphan with regards support,

How did you obtain the SDK that you used?.

Your help much appreciated.

Regards Noel.

0 Kudos

965 Views
nxf58474
NXP Employee
NXP Employee

Hi Noel,

 

You can download the SDK from the MCUXpresso SDK Builder.

 

You are right, there is no evaluation board for MK22FX512Axxx12, but there is the SDK for the processor:

 

pastedImage_2.png

This means that the SDK doesn't have SDK examples, but it includes the Drivers you can use for your project.

pastedImage_4.png

 

Hope this helps.

 

Best Regards,

Ricardo

0 Kudos

965 Views
divner
Contributor I

Hi Ricardo.

Thank you for all the info.

I am currently learning how to use MCUXpresso with the objective of using the Config Tools

to create a custom Project for the Mk22FX512. I am progressing reasonably well.

I am requiring to be able to enter Deep Sleep Mode and the wake up as required.

Thanks again for your help.

Best Regards Noel.

0 Kudos